To mount the controller, complete the following steps:
- Mount a 20 cm (8 in.) section of 35 mm (1.3 in.) DIN rail horizontally.
Note: Mount the controller in the horizontal position.
- On the back of the controller, extend the two mounting clips as shown in the following figure.
Figure 1. Pull lower mounting clips down
- Place the controller on the DIN rail.
- To secure the controller on the DIN rail, push the bottom mounting clips up as shown in the following figure.
Figure 2. Push lower mounting clips up
- To remove the controller from the DIN rail, pull the bottom mounting clips out to the extended position and carefully lift the controller off the DIN rail.