The following table describes the System Configuration menu on the Smart Building Hub (SBH).
Menu option | Description | Range |
---|---|---|
Supply Fan Type |
Sets whether the fan is constant volume or uses a fixed variable strategy |
Adjustable:
|
Fan Cycling |
Allows the fan to cycle off |
Adjustable:
|
Cooling Device Type |
Sets the type of cooling the device uses |
Adjustable:
|
Number of Cooling Stages Installed |
If you set the cooling device type to Staged, use this parameter to set the number of stages. |
Adjustable: 0-4 |
Number of Heat Pump Stages Installed |
If you set the cooling device type to Heat Pump, use this parameter to set the number of stages. |
Adjustable: 1-2 |
Heating Device Type |
Sets the type of heating the device uses |
Adjustable if non-heat pump:
Adjustable if heat pump:
|
Number of Heating Stages Installed |
If you set the heating device type to Staged, this parameter sets the number of stages |
Adjustable: 0-4 |
Number of Supp Heating Stages Installed |
If you set the heating device type to Heat Pumpwith supplemental heating, this parameter sets the number of supplemental heat stages |
Adjustable: 1-2 |
Economizer Damper Type |
This allows the system to define an economizer or a minimum outside air damper. |
Adjustable:
|
Economizer Fault Detection |
Enables the economizer fault detection diagnostic sequences |
Adjustable:
|
Humidity Enable |
Enables the humidity control sequences |
Adjustable:
|
Dehumidification Enable |
Enables the dehumidification control sequences |
Adjustable:
|
Heat Cool Diagnostics |
Enables the heat cool alarms. The heat cool alarms use a supply air sensor to determine if the heating or cooling is working correctly. |
Adjustable:
|
No. | Description | |
---|---|---|
1 |
Mixed air damper output |
|
2 |
Speed control for supply fan |
|
Staged unit |
Heat pump |
|
3 |
Fan |
Fan |
4 |
Heating stage 1 |
Supplemental heating stage 1 |
5 |
Heating stage 2 |
Supplemental heating stage 2 |
6 |
Cooling stage 1 |
Compressor 1 command |
7 |
Cooling stage 2 |
Compressor 2 command |
8 |
Cooling stage 3 |
Reversing valve |
9 |
Cooling stage 4 |
Not used |
10 |
24 VAC COM |
24 VAC COM |
11 |
24 VAC |
24 VAC |
12 |
Mixed air damper output |
|
13 |
24 V HOT power transformer |
|
14 |
From last device |
|
15 |
To next device |
|
16 |
NS zone sensor. May have many options. Required if you do not control from RA-T sensor |
|
17 |
Optional. Zone sensor. Connector on the back of the sensor. Wire the sensor bus to any other network sensors in a daisy-chain configuration. |
|
18 |
Optional. Return air temperature. Can be used to control instead of a zone temperature sensor. |
|
19 |
Mixed air damper feedback. Required for Title 24 economizer fault detection diagnostics. |
|
20 |
Optional. Outside air temperature. For a hardwired sensor. You can also data share the outside air temperature. |
|
21 |
Mixed air temperature. Required if you have proportional heating or cooling and an economizer. |
|
22 |
Supply air temperature. Required if you have an economizer and no mixed air temperature. |
|
23 |
Service alarm. Optional. Dry contact input used to give a general service alarm. |
|
24 |
Occupancy sensor. Optional. Used to reset setpoints when the room is unoccupied. |
|
25 |
Low temperature alarm. Required when you have water coils and an economizer. |
|
26 |
Fan status. Optional. |
No. |
Description |
|
---|---|---|
1 |
Continuation of unit terminal strip: Heating stage 3 |
|
2 |
Continuation of unit terminal strip: Heating stage 4 |
|
3 |
Continuation of unit terminal strip: 24VAC |
|
4 |
Hot gas bypass solenoid |
|
5 |
Humidifier: output 0 VDC - 10 VDC |
|
6 |
Humidifier enable |
|
7 |
Cooling output |
|
8 |
Heating output |
|
9 |
Humidifier high limit: Control signal out |
|
10 |
Humidifier high limit: Control signal in |
|
11 |
Humidifier high limit: Common |
|
12 |
Humidifier high limit: 24 VAC |
|
13 |
24 V COM power transformer |
|
14 |
24 V HOT power transformer |
|
15 |
Sensor bus. Wire to the sensor bus on the VAC1000 in a daisy-chain configuration |
|
16 |
Optional sensor: Purge command |
|
17 |
Optional sensor: Filter status |
|
18 |
Optional sensor: Return air CO2 |
|
19 |
Optional sensor: Zone humidity |