Configuring a one-condition interlock - Verasys - LIT-12012533 - LC-SBH200-0 - Building automation software - Verasys System - 4.0
Verasys System European User's Guide
- Brand
- Verasys
- Product name
- Verasys System
- Document type
- User Guide
- Document number
- LIT-12012533
- Version
- 4.0
- Revision date
- 2020-10-30
- Product status
- Active
- Language
- English
Procedure
-
On the Interlock Condition area, from the Device
drop-down list select the device that you want to associate with the interlock to
show all the points you can assign between the device and the interlock.
-
From the Points drop-down list, select the Point you want to
associate with the interlock. This action makes the point part of the Interlock
logic.
-
From the Operator drop-down list, select the operator for the point.
-
Enter the value.
-
Enter the Differential +/- variance.
-
Under Input Conditions, select One Condition.
-
In the Interlock Action area, select the device and point on which you
want to perform the interlock action. You can configure an action when the interlock
is true or false.
-
Click Save to enable the interlock.