To edit standard graphics on a SMART Device, complete the following steps:
- Click Devices.
- Select the device that you want to change the graphics on.
- To change the graphic, select the Change Graphic button on the devices homepage.
- On the Change graphics home page, navigate to Uploaded Images.
- Choose an existing image or select the Upload button to upload your own graphic. The graphic must be under 15 megapixels and less than 10 MB.
- Click Apply.