About this task
If you have a certificate from a public CA, import it using the following procedure:
Procedure
- In the Certificates dialog box, click the Trusted Root Certification Authorities tab.
- Click Import.
- In the Certificate Import Wizard dialog box, click Next.
- Browse to the rootCA.pem security certificate file and select it.
- Click Open.
-
Click Next.
Note: Install the rootCA.pem file and not the www.smartbuildinghub.com file that the browser prompts you to install. The rootCA.pem file certifies your device for any SBH you use. If you install the www.smartbuildinghub.com file that the browser prompts you to install instead, you need to add a new certificate for each new SBH device that you use.
- On the Certificate Store page of the Wizard, select Place all certificates in the following store.
- Verify that the certificate store listed is Trusted Root Certification Authorities.
- Click Next.
- The Completing the Certificate Import Wizard appears, Click Finish.
- In the Security Warning dialog box, click Yes.
- Click OK to close the Wizard.