About this task
These instructions are for additional settings that are required when connecting the SBH to an Ethernet network. These settings occur after the steps in Connecting to the SBH for the first time.
Important: When using the SBH on Ethernet, you must plug it into external power before you attach the field bus adapter.
Procedure
Results
You can use static or manual settings rather than automatic settings with your SBH. However, if you do so, you must contact your IT department for all necessary manual settings to ensure that your SBH works on your company's network.