About this task
Important: If you are going to use the Smart Building Hub on Ethernet, you must plug it into external power before you attach the field bus adapter.
The following instructions are based on the information in the Quick Start Guide (Part No. 24-10737-00229) that comes with each SBH. The default login credentials for each SBH are included in the Quick Start Guide that ships with each device.
Procedure
Results
You can now use your SBH through the Wi-Fi connection. If you are connecting your SBH to an Ethernet network, continue to Connecting the SBH to Ethernet.