LED test sequence at startup - Verasys - LC-SBH200-0 - LC-SBH200-0E - LC-SBH200-0LA - LC-SBH200-0S - Supervisory Device - SBH200

Verasys Smart Building Hub (SBH) Installation Guide SBH200

Brand
Verasys
Product name
SBH200
Document type
Installation Guide
Part number
24-10737-00237
Document revision
C
Revision date
2020-01-17
Language
English

During startup, the SBH automatically initiates a self test to verify correct operation. Immediately after you connect the supply power, the following LED lighting sequence occurs:

  • The POWER LED starts on purple and then turns blue and stays on.
  • The FAULT LED flashes for approximately 30 seconds, then turns off and the RUN LED turns solid when the SBH is fully functional.
  • The Wi-Fi LEDs remain off until you connect the Wi-Fi dongle. When you connect the Wi-Fi dongle, the corresponding USB LED turns on and the Wi-Fi AP LED flickers, which indicates that the SBH is waiting for a device.