Procedure
- The SBH permanently connects to the Verasys system using the four-terminal system bus port. Wire the system bus communications to the blue, four-terminal connector and connect to the port as shown in the following figure.
-
If the SBH is at the end of a line, set the end-of-line (EOL) switch to ON.
Figure 1. Connecting the SBH to your equipment
- Connect the Wi-Fi adapter to either of the USB ports.
- Connect the RJ45 Ethernet port to the building Ethernet network. Use instructions from the building IT department.
- In the Wi-Fi settings of your device or laptop, connect to the SBH Wi-Fi network using the default credentials. You can find the default credentials on a sticker on the Smart Building Hub Quick Start Guide (Part No. 24-10737-00229) that came with the SBH. You can also find the default credentials on a sticker on the back of the SBH.
-
To open the SBH browser interface, direct your browser to www.smartbuildinghub.com.
Note: The SBH ships with a private www.smartbuildinghub.com SSL certificate installed to ensure secure communication. However, this certificate does not indicate that it is trusted in a browser. If you want to install your own certificate, refer to Adding a Private Key and Certificate to Smart Building Hub in the Smart Building Hub Network and IT Guidance Technical Bulletin (LIT-12012324).
- Read and accept the SBH license agreement.
-
The first time you log in to the SBH, the Change Password and Passphrase page appears. You must change the admin password and Wi-Fi passphrase.
Important: After you change the Wi-Fi passphrase or SSID, the web server restarts and you must rejoin the SBH Wi-Fi network using the new passphrase. On some mobile devices, you must select and forget the original SBH Wi-Fi network before you rejoin the network with the new passphrase. For example, on a laptop running a Microsoft® Windows® operating system, you must select and forget the original Wi-Fi network before you rejoin.
- In the New Admin Password field, replace the default password. Enter the new password in the Verify New Admin Password field to confirm the change.
- In the New Wi-Fi Passphrase field, replace the Wi-Fi passphrase and click Save.
- To see and interact with a device on the network, use the web-enabled device or laptop that is connected to the SBH Wi-Fi network.
Results
When you physically connect the SBH to the MS/TP network, all the devices on the network that have unique addresses appear in the device list and are available to configure.