Field Bus Communications Connections - Verasys - LC-SBH100-0 - Supervisory controller - SBH100

Verasys Smart Building Hub (SBH) Installation Guide LC-SBH100-0

Brand
Verasys
Product name
SBH100
Document type
Installation Guide
Part number
24-10737-113
Document revision
D
Revision date
2021-03-26
Product status
Active
Language
English

To connect the Smart Building Hub to the FC field bus for communication, connect the RJ-12 cable to the Smart Building Hub and wire the other end to the FC bus using the field adapter connector.

Note: The Smart Building Hub has a dedicated MS/TP bus address of 03. The number of Smart Building Hub units that can be connected simultaneously to one MS/TP bus depends on the number of FC ports available and connected to the bus. The MS/TP bus can accommodate one Smart Building Hub on the FC bus.
Note: Performance of the Smart Building Hub varies based on the amount of traffic.