LED Test Sequence at Startup - Verasys - LC-SBH100-0 - Supervisory controller - SBH100

Verasys Smart Building Hub (SBH) Installation Guide LC-SBH100-0

Brand
Verasys
Product name
SBH100
Document type
Installation Guide
Part number
24-10737-113
Document revision
D
Revision date
2021-03-26
Product status
Active
Language
English
During startup, the Smart Building Hub automatically initiates a self-test to verify proper operation of the unit. Immediately after connecting supply power, the following LED lighting sequence occurs:
  • The power LED turns on, and stays lit.
  • The Fault LED indicator flashes for approximately 40 seconds, then turns off when the Smart Building Hub is fully functional.
  • The Wi-Fi LEDs light up in succession (scanning), indicating that the Smart Building Hub is waiting for a device to join its Wi-Fi network.