Special Tools Needed - Verasys - LC-SBH100-0 - Supervisory controller - SBH100

Verasys Smart Building Hub (SBH) Installation Guide LC-SBH100-0

Brand
Verasys
Product name
SBH100
Document type
Installation Guide
Part number
24-10737-113
Document revision
D
Revision date
2021-03-26
Product status
Active
Language
English

To use the Smart Building Hub, you need a mobile device (tablet or Smart phone) or computer (laptop or desktop) that supports Wi-Fi.

If the unit is mounted to a vertical surface without a DIN rail, you need screws to mount the unit. The specific screw types depend upon the surface to which the unit is mounted. The screw holes on the Smart Building Hub can accommodate M3.5 and #6 screws.

Use of the mounting bracket locking screw requires a T15 Torx driver.