The table below provides troubleshooting information for the Graphic Generation Tool application.
Problem |
Solution |
---|---|
When you install the Graphic Generation Tool, you see a message stating that an Admin user profile is required. |
Exit the installation program and install the software using a computer account that has Administrator privileges. Note: The installation log includes information about error
messages that you may encounter when you install the Graphic
Generation Tool. This information may help you resolve an
error message. You can find the installation log in the
following locations.
Windows 7 and Windows Server 2008 R2: C:\Users\<user name>\AppData\Roaming \GraphicToolInstallLog.html |
When you install or upgrade the Graphic Generation Tool, the following error message appears:
|
Save your work and close the Graphic Generation Tool application. Then, click Retry in the message box or start the installation program again. Follow the instructions in Upgrading the Graphic Generation Tool. |
You are installing .NET Framework 4.0 on a computer running other Metasys software, and the Metasys software stops running. |
Restart the computer.
Note: If a disruption occurs on the SCT or
on the Ready Access Portal, restart this device as well.
|
You are installing .NET Framework 4.0 on a computer that already has this application installed. The following dialog box appears: |
Close this dialog box by clicking the X in the upper right corner of the screen. Continue installing. |
When you attempt to update the System Configuration Tool (SCT) or the Application and Data Server (ADS) with the latest Graphics+ Package via the Update Metasys Hosts command in the Graphic Generation Tool (GGT), you may receive an error at 99%. The Graphics+ Package does not update. This error occurs with the SCT or the ADS at Metasys® Release 5.2 with a Graphics+ Package for Release 1.1 or 1.2. or You are a Metasys for Validated Environment (MVE) site and branch laptops or external storage devices cannot be connected to the SCT or ADS. |
To manually update the SCT or ADS with the latest Graphics+ Package:
|