Note: Use the following procedure to change the language used for menus, messages,
and tool tips in the Graphic Generation Tool. The LIP tool is required for these
steps.
Procedure
Using the LIP tool, add any languages you need to support.
Start GGT.
Click theView > Options menu item. The Options dialog box
appears.
Figure 1. Language Options Selection
Click the Language tab.
In the Display Language field, select your language.
Click Save, and then click OK in the Changing Language alert
box.
Figure 2. Language Change Confirmation
Restart the GGT for the language change to take effect.