In the upper right of the UI, click on the User profile icon to go to the Account Settings page. Perform the following actions on the Account Settings page:
- To add or edit an email address, in the Email field, type an email address, and click Save.
- To select a time zone, from the Time zone list, select your time zone, and click Save.
- To select the unit of measurement, from the Unit of measurement list, select a unit of measurement, and click Save.
- To select the language, from the Language list, select your preferred language, and click Save.
- To add or edit your telephone number, in the Mobile Number field, enter your mobile number in the international format, and click Save.
You can also change your password from the Account Settings page. For more information, see Changing your password.