About this task
On the Device List screen in Verasys, you can view the devices that are online and connected to the SBH. If the zone coordinator is connected and online, it appears on the Device List screen. See Figure 1.
- The white address square beside a device indicates that it is wired to the zone bus.
- The blue address square beside a device indicates that it is wired to the system bus.
The zone coordinator appears on the system bus. The devices on the zone bus appear under the zone coordinator. The Device List screen shows the devices that are connected and if they are online.
Figure 1. Device list screen in Verasys
Number | Description |
---|---|
1 | Device list screen |
2 | The white address square beside a device indicates that it is wired to the zone bus. |
3 | The blue address square beside a device indicates that it is wired to the system bus. |