The Verasys 18 point 24V Application Controller is part of the SMART Equipment controller family. Verasys Application Controllers run pre-engineered applications and provide the inputs and outputs required to monitor and control a wide variety of HVAC equipment.
Verasys Application Controllers operate on an RS-485 BACnet® (MS/TP) Bus as BACnet Advanced Application Controllers (B-AACs) and integrate into Johnson Controls® and third-party BACnet systems.
Verasys Application Controllers include an integral real-time clock, which enables the controllers to monitor and control schedules, calendars, trends, and operate for extended periods of time as stand-alone controllers when offline from the system network.
Important: Use this Verasys Application Controller only as an operating control. Where failure or malfunction of the Verasys Application Controller could lead to personal injury or property damage to the controlled equipment or other property, additional precautions must be designed into the control system. Incorporate and maintain other devices, such as supervisory or alarm systems or safety or limit controls, intended to warn of or protect against failure or malfunction of the Verasys Application Controller.
Important : Utiliser ce Verasys Application Controller uniquement en
tant que dispositif de contrôle de fonctionnement. Lorsqu'une défaillance ou un
dysfonctionnement du controller risque de provoquer des blessures ou d'endommager
l'équipement contrôlé ou un autre équipement, la conception du système de contrôle doit
intégrer des dispositifs de protection supplémentaires. Veiller dans ce cas à intégrer
de façon permanente d'autres dispositifs, tels que des systèmes de supervision ou
d'alarme, ou des dispositifs de sécurité ou de limitation, ayant une fonction
d'avertissement ou de protection en cas de défaillance ou de dysfonctionnement du
Verasys application controller.