Notifier detectors - Simplex - Non-addressable fire alarm control unit - 05791417

2004 and 2008 Foundation Series Fire Alarm Control Unit Two Wire Detector Compatibility Chart

Document Number
05791417
ft:locale
en-US
Document Revision
Rev. B
Table 1 contains a list of compatible Notifier detectors.
Table 1. Notifier detectors
Detector Description Bases Fire Alarm Control Units
2004 2008
SD-651 {A} Photo B401, B610LP {A} 16 25
Note:
  1. The compatibility identifier is in { } brackets and shown after the detector and base model number.
  2. Do not use these devices on a zone that is programmed for alarm verification.
  3. When you use accessories, use only one detector on an IDC.