Zone bus terminal block - Verasys - Field Device - Verasys ZEC510 Variable Air Volume Controller

Verasys ZEC510 VAV Controllers Installation Guide

Product
Variable Air Volume > Variable Air Volume Controls > Verasys ZEC510 Variable Air Volume Controller
Document revision
B
Revision date
2021-04-08
Product status
Discontinued
docpartnumberlabel
Part No.
Part number
24-10143-01485

The zone bus terminal block is a gray, removable, 4-terminal plug that fits only into the black, board-mounted, zone bus jack. Wire the removable zone bus terminal block plugs on the ZEC510 and other zone bus controllers in a daisy-chain configuration using 3-wire twisted, shielded cable, as shown in Figure 1 and Figure 2.

Figure 1. Zone bus terminal block wiring

Figure 2. Zone bus daisy chaining configuration

Table 1. Zone bus daisy chaining configuration
1 Terminating device on the zone bus
2 Zone bus terminal block plug on the terminating device
3 Daisy-chained device on a zone bus segment
4 Zone bus terminal block plug on the daisy-chained device
5 Cable shield connection
6 Connects to the next device on the zone bus. Connects to all ZECs and the zoning roof top unit (RTU) of the VZC100.