Modular ports - Verasys - Field Device - Verasys ZEC510 Variable Air Volume Controller

Verasys ZEC510 VAV Controllers Installation Guide

Product
Variable Air Volume > Variable Air Volume Controls > Verasys ZEC510 Variable Air Volume Controller
Document revision
B
Revision date
2021-04-08
Product status
Discontinued
docpartnumberlabel
Part No.
Part number
24-10143-01485

The modular sensor and zone bus ports on the front of the ZEC510 are RJ12, six-position, modular jacks. The modular sensor bus ports provide a connection for the VAV Balancing Tool. The zone bus port is not used in ZEC510 installations. The following figure shows the pin number assignments on the modular port.

Figure 1. Pin number assignments

Table 1. Pin number assignments
1 Power 15 VDC
2 Bus and power common
3 Power 15 VDC
4 Bus and power common
5 Sensor or zone bus -
6 Sensor or zone bus +