Use the following diagrams and tables to address the NS sensors.
Figure 1. CO2 net stat with terminals addressable
A | Address switch |
B | To next device on the sensor bus if required |
C | From previous device on the sensor bus |
Available DIP switch addresses | DIP switch settings | ||
---|---|---|---|
Switch 4 | Switch 2 | Switch 1 | |
212 | Off (open) | Off (open) | Off (open) |
213 | Off (open) | Off (open) | On (closed) |
214 | Off (open) | On (closed) | Off (open) |
215 | Off (open) | On (closed) | On (closed) |
216 | On (closed) | Off (open) | Off (open) |
217 | On (closed) | Off (open) | On (closed) |
218 | On (closed) | On (closed) | Off (open) |
219 | On (closed) | On (closed) | On (closed) |
Figure 2. NS sensors with terminals addressable
1 | Thermostat circuit board Note: Jack J2 is for
commissioning tools.
|
2 | Address switch |
3 | Terminal block on the NS sensor. Connector on the mounting base slides into W4 pins on the circuit board |
4 | To next device on the sensor bus if required |
5 | From previous device the on the sensor bus |
Available DIP switch addresses | DIP switch settings | ||
---|---|---|---|
Switch 4 | Switch 2 | Switch 1 | |
199 | Off | Off | Off |
200 | Off | Off | On |
201 | Off | On | Off |
202 | Off | On | On |
203 | On | Off | Off |
Note: Addresses 204 to 206 are not supported.