The ZEC510 VAV controller is a component of the Verasys SMART Equipment
family. The ZEC510 variable air volume (VAV) controller runs a pre-engineered HVAC
zoning sequence and provides the inputs and outputs you require for VAV
applications.
The ZEC510 controller has an optional occupancy feature that makes it possible for the
controller to switch from occupied mode to standby mode based on zone activity. Standby
mode maximizes energy savings by using setpoints that are higher and lower than occupied
mode setpoints.
The ZEC510 controller uses plug and play technology to detect which network sensor types
are connected. See Accessories for additional sensor
information.
Use the Verasys Smart Building Hub (SBH) to configure the ZEC510 controller. Use the SBH
or the VAV Balancing Thermostat to commission the controller.
Important: Use this ZEC510 VAV controller only as an operating control. Where
failure or malfunction of the ZEC510 controller could lead to personal injury or
property damage to the controlled equipment or other property, additional precautions
must be designed into the control system. Incorporate and maintain other devices, such
as supervisory or alarm systems or safety or limit controls, intended to warn of or
protect against failure or malfunction of the ZEC510 VAV controller.
Important: Utiliser ce ZEC510 VAV controller uniquement en tant que dispositif
de contrôle de fonctionnement. Lorsqu'une défaillance ou un dysfonctionnement du
controller risque de provoquer des blessures ou d'endommager l'équipement contrôlé ou un
autre équipement, la conception du système de contrôle doit intégrer des dispositifs de
protection supplémentaires. Veiller dans ce cas à intégrer de façon permanente d'autres
dispositifs, tels que des systèmes de supervision ou d'alarme, ou des dispositifs de
sécurité ou de limitation, ayant une fonction d'avertissement ou de protection en cas de
défaillance ou de dysfonctionnement du ZEC510 VAV controller.