Sensor bus terminal block - Verasys - LC-ZEC310-0 - LC-BYP200-0 - Bulb controller - Verasys ZEC310 Zone Damper

Verasys ZEC310 Zone Damper and BYP200 Bypass Damper Controllers Installation Guide

Product
Dampers > Zone Dampers > Verasys ZEC310 Zone Damper
Document revision
D
Revision date
2019-07-01
Product status
Discontinued
Part number
24-10143-1248

The sensor bus terminal block is a brown, removable, 4-terminal plug that fits only into the brown, board-mounted sensor bus jack. Wire the removable sensor bus terminal block plugs on the ZEC310 and other field devices in a daisy-chain configuration using a 4-wire twisted, shielded cable as shown in the following figure.

Figure 1. Sensor bus terminal block wiring

Figure 2. Sensor bus daisy chaining configuration

Table 1. Sensor bus daisy chaining configuration
Callout Description

1

Terminating device on the sensor bus

2

Sensor bus terminal block plug on the terminating device

3

Daisy-chained device on a sensor bus segment

4

Sensor bus terminal block plug on the daisy-chained device

5

Cable shield connection

6

Connects to the next device on the sensor bus. Connects tothe NS-xxxx sensors. See the Accessories section for a listof the NS-xxxx sensors.