Using as a router connected to a MS/TP Controller - Verasys - LIT-12014167 - LC-TMR100-0 - Wireless Device - TMR Series Wireless Router Installation Guide - 4.2

Verasys TMR Series Wireless Router Installation Guide

Brand
Verasys
Product name
TMR Series Wireless Router Installation Guide
Document type
Installation Guide
Document number
LIT-12014167
Version
4.2
Revision date
2023-09-06
Language
English
  1. Connect the TMR to a compatible Field Controller using the FC Bus RJ-12 connector. This connection provides both power and communication to the TMR.
  2. Alternately, connect the + and – screw terminals on the TMR to the MS/TP RS485 + and – connections on the MS/TP controller and connect the 9-24VAC/VDC and GND screw terminals on the TMR to a compatible power source, see Figure 2.
Figure 1. RJ-12 pin out on the controller
Note: See Verasys BACnet MS/TP Communications Technical Bulletin (LIT-12012362) for more information.
Figure 2. TMR wired to a MS/TP controller by a screw terminal
Figure 3. TMR wired to an VZC100 Verasys Zone Coordinator with an RJ-12 cable
Note: When connecting to the System bus, it is best practice to hard-wire the SBH200 to the VZC100.
Figure 4. TMR wired to VEC100 controller
Note: VEC controllers do not have an RJ-12 plug for their Zone Bus. This requires you to discretely wire the controller to the TMR. Connect the TMR + and - signals to the Zone Bus connector and TMR PWR/COM signals to the Sensor Bus connector. Alternately you can connect the PWR and COM to the 24V-OUT terminals.
Figure 5. VEC100 controller wiring diagram
Figure 6. TMR wired to VAC100x controller