TMR State | Color | Description |
---|---|---|
Off Network |
Blue/green blip |
Restarting or searching for PAN to join |
On Network - Normal State |
Green1,2 Yellow1,2 |
Router mode - green Coordinator mode - yellow PAN closed for joining |
On Network - Commissioning State |
Red1 |
PAN open for joining |
On Network - Warning State | Purple1,2 | Warning:
|
Dim purple | Warning:
|
|
Miscellaneous |
Aqua1 |
Firmware update in progress |
White blink at 1 Hz rate and stopping after 30 seconds | Response to a ping request from the SBH200 local UI |
Note:
1
Blink rate is an indication of signal quality. 1 - Poor, 2 - Fair, 3 - Good.
Note:
2
Blinking stops 5 minutes after reset.