MS/TP baud rate - Verasys - LIT-12014167 - LC-TMR100-0 - Wireless Device - TMR Series Wireless Router Installation Guide - 4.2

Verasys TMR Series Wireless Router Installation Guide

Brand
Verasys
Product name
TMR Series Wireless Router Installation Guide
Document type
Installation Guide
Document number
LIT-12014167
Version
4.2
Revision date
2023-09-06
Language
English

The TMR attempts to synchronize its baud rate to the MS/TP Bus. The TMR supports baud rates of 9600, 19.2k, 38.4k, and 78.6k.

When in Router Mode, if there is no bus activity seen approximately 10 seconds after power up, the TMR starts the MS/TP Token ring at 38.4k baud.

When in Coordinator Mode, the TMR does not start the MS/TP Token Ring and remains in an auto-baud mode waiting for the connected SBH200 or VZC to start the Token Ring.