About this task
After properly mounting, wiring, and setting the AREA/PAN OFFSET switches, complete the following steps to add a new device to the TMR wireless network:
Procedure
- Apply power to the SBH200 and TMR.
- Verify the TMR is in Coordinator Mode (Yellow LED).
- Momentarily press the Join Push button on the TMR Coordinator or from the SBH200 UI to open the Wireless Network.
- Verify the network is open (Red LED).
- Apply power to the remote MS/TP Equipment/TMR.
- Verify the TMR is wired to controller and the TMR is in router mode (Green LED).
- Within one minute the network is open, the TMR Router joins the Wireless Network (Red LED).
- Verify the RF signal quality (LED Blink pattern).
- Verify the MS/TP Equipment is discovered in the SBH200 UI.
- After approximately one hour, the wireless network automatically closes and the TMR LEDs on the wireless network return to their normal state.
-
To verify signal quality, quickly press or release the Join
Push button on the TMR Router. The LED blinks the signal quality.
Note: It takes up to 15 seconds for the TMR to enter the Normal State (Green or Red LED). If the TMR remains in a Warning State (Purple LED), further investigation is required.Note: After initially joining the Wireless Network, the TMR may automatically receive a firmware update if required (Aqua LED). It may take up to 15 minutes to complete the firmware update.Note: If the TMR does not enter the correct Coordinator or Router mode, Yellow LED or Green LED respectively, you may need to manually set the mode. See Table 1.