North American emissions compliance - Verasys - LIT-12014167 - LC-TMR100-0 - Wireless Device - TMR Series Wireless Router Installation Guide - 4.2

Verasys TMR Series Wireless Router Installation Guide

Brand
Verasys
Product name
TMR Series Wireless Router Installation Guide
Document type
Installation Guide
Document number
LIT-12014167
Version
4.2
Revision date
2023-09-06
Language
English

United States

Compliance Statement (Part 15.19)

This device complies with Part 15 of the FCC Rules. Operation is subject to the following two conditions:

  1. This device may not cause harmful interference, and

  2. This device must accept any interference received, including interference that may cause undesired operation.

Warning (Part 15.21)

Changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate the equipment.

RF Exposure

To comply with FCC RF exposure requirements for mobile transmitting devices, this transmitter should only be used or installed at locations where there is at least 20 cm separation distance between the antenna and all persons.

Canada

Industry Canada Statement(s)

This device complies with Industry Canada licence-exempt RSS standard(s). Operation is subject to the following two conditions:

  1. This device may not cause interference, and

  2. This device must accept any interference, including interference that may cause undesired operation of the device.

ISED Radio Frequency (RF) Exposure: This equipment complies with FCC and ISED Canada radiation exposure limits set forth for an uncontrolled environment. The user should avoid prolonged exposure within 20 cm of the antenna, which may exceed the FCC or RSS-102 radio frequency exposure limits.

Exposition aux fréquences radio (RF) de la ISDE : Cet équipement se conforme aux limites d'exposition aux radiations de la FCC et de ISDE Canada, établies pour un environnement non contrôlé. L'utilisateur doit éviter une exposition prolongée à moins de 20 cm de l'antenne, qui peut dépasser les limites d'exposition aux fréquences radio FCC ou RSS-102.

Le présent appareil est conforme aux CNR d'Industrie Canada applicables aux appareils radio exempts de licence. L'exploitation est autorisée aux deux conditions suivantes :

  1. L'appareil ne doit pas produire de brouillage, et

  2. L'utilisateur de l'appareil doit accepter tout brouillage radioélectrique subi, même si le brouillage est susceptible d'en compromettre le fonctionnement.