The TMR Wireless Router (TMR) is a component of the Verasys Controls System which provides wireless connectivity to BACnet® MS/TP controllers, including Verasys Simplicity Smart Equipment Rooftops, VAC, VEC TEC, VZC, ZEC, and third-party controllers, over a wireless mesh network. The TMR can be used as a wireless Network Coordinator, a Router, or a stand-alone repeater.
The Verasys Smart Building Hub (SBH) automatically recognizes the TMR as a wireless network coordinator on the Verasys System (FC) Bus. The Verasys Zone Coordinator (VZC) automatically recognizes the TMR as a wireless network coordinator on the Verasys Zone (CS) Bus.