Indoor line-of-sight transmission ranges between products can vary greatly from the data in the Table 1. The effective transmission range or distance for indoor applications also varies because of wireless signal absorption and reflection due to metal obstructions, walls, floors, and furniture found in typical building interiors.
For more information, refer to the Verasys TMR Series Wireless Best Practices (LIT-12014163).
Range type | Transmission distance | |
---|---|---|
TMR to TMR 100mW versions | ||
Recommended | 250 ft (75 m) | |
Maximum, line of sight | 1000 ft (300 m) | |
Maximum, through multiple hops | 2000 ft (600 m) |