Applications - Verasys - LIT-12014167 - LC-TMR100-0 - Wireless Device - TMR Series Wireless Router Installation Guide - 4.2

Verasys TMR Series Wireless Router Installation Guide

Brand
Verasys
Product name
TMR Series Wireless Router Installation Guide
Document type
Installation Guide
Document number
LIT-12014167
Version
4.2
Revision date
2023-09-06
Language
English
Important: Where failure or malfunction of a TMR or loss of communications due to wireless interference could lead to personal injury or property damage to the controlled equipment or other property, additional precautions must be designed into the control system. Incorporate and maintain other devices, such as supervisory or alarm systems, or safety or limit controls, intended to warn of or protect against failure or malfunction of a TMR.
Important: The TMR Series Wireless System is not designed or intended for use in mission-critical or life-safety applications.