Configuring a schedule - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

Procedure

  1. Click Schedules > Add New Schedule.
  2. Enter a new schedule name. The new schedule status defaults to Enabled.
  3. Select the Analog or Multistate schedule data type from the drop down list.
  4. Configure additional parameters based on the schedule data type:
    • For analog schedules, select the display units and display precision from the drop-down menus.
    • For multistate schedules, select the schedule type from the drop-down menu. The available schedule types are Off/On, Occupied/Unoccupied, or Occupied/Unoccupied/Standby/Not Set.
  5. Select the scheduled objects that you want to control with this time schedule and click Save. The list of objects depends on the connected devices and on the schedule type selected.
  6. Click +Add. A separate page appears where you can add events for the schedule. Click the Clock icon to set a time. Select a status and the days, and click Save.
    Note: You set the time in the 24-hour format and the time field converts it to the standard 12-hour time format with AM and PM adjusted.
    Important: When you save a weekly event, the schedule is not yet saved. Continue with the next step to save the schedule.
  7. Click Save to save the new schedule.