ZEC firmware download - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

You can use the ZEC firmware download feature to upgrade all the zone controllers in a zoning system through the USB upgrade of the Verasys Zone Coordinator (VZC100). This feature means future enhancements to the zone controllers are possible without physically replacing the hardware. The firmware download supports the following zone controller devices:

  • LC-BYP200-0
  • LC-ZEC310-0
  • LC-ZEC410-1
  • LC-ZEC410-2
  • LC-ZEC410-3
  • LC-ZEC510-x
Note: The download process takes between five and seven minutes for each zone.