Testing the unit - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
User Guide
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

To test the unit, navigate to the VEC Commissioning page and complete the following steps:

  1. Set the Start Commission parameter to Trigger.
  2. Block zones open.
  3. Turn on the fan.
  4. If the unit has heating capability, turn on heating stages and ensure the SAT increases. Most VAV systems do not have heat, but if your system does have heat, you need to install a return air sensor that can control the heat for warm-up mode.
  5. Turn on cooling stages and ensure the SAT decreases.
  6. Set the Start Commission parameter back to Normal to finish unit testing.