Configuring a Smart Equipment unit for VAV system using the SBH - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

The Smart Equipment unit is delivered with partial factory setup completed. Follow this procedure to check that the minimal settings have been performed.

  1. Log on to the SBH.
  2. From the device list screen, select the Smart Equipment unit. The RTU home page and the RTU menu structure appear.
  3. Navigate to Controller > Description.
  4. Set Rooftop Controller Type to VAV. If it is not set to VAV, the zone coordinator does not control as a VAV system.
  5. Navigate to Details > Indoor Fan > Setup, and verify that Fan Control Type is set to Variable Speed.
    Note: In older versions of Smart Equipment firmware, Rooftop Controller Type is located in the Details > Service > Factory > Miscellaneous section, and Fan Control Type is located in Details > Service > Factory.
  6. Check the operation of the unit. Use the steps in the Setting the temperature control and flow parameters section to complete the configuration.
    Note: Ensure you have some zones blocked open to relieve duct pressure.