Configuring zone groups for scheduling - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

About this task

Group schedules is a feature in the zone coordinator to simplify the creation of zone controller schedules. You can assign each zone controller to one of four zone groups, and you can create a schedule for each zone group in the zone coordinator. This way, you can create the same schedule and add exceptions for multiple zone controllers. Refer to the following video link https://docs.jci.com/bas/verasys-zone-groups-scheduling.

Note: By default, zone controllers are in zone group 1 until you move them to a different group.

Procedure

To assign a zone controller to a zone group, complete the following steps:

  1. Select the controller device.
  2. Click Control Setup.
  3. In the Zone Group Number field, enter the zone group number in the range of 1 to 4.

What to do next

Assign all zone controllers to a zone group. When you create a schedule for the zone coordinator, you can also select the zone group that you want to add the schedule to.