VAV controller zone setup procedures - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
User Guide
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

The Verasys zone controllers come with predefined parameters and are easy to configure when they communicate to the zone coordinator. However, you need to configure temperature control and flow control to ensure proper operation and control of the equipment connected to the devices. This section instructs you on how to set up the zone controllers for temperature and flow control. Refer to Verasys ZEC510 VAV Controllers Installation Guide Part No. 24-10143-01485.