Configuring binary and analog inputs - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

To configure binary and analog inputs, complete the following steps:

  1. Navigate to the Commissioning tab and select the Inputs tab.
  2. On the Generic IOM Inputs screen, configure the following fields:
    • Set the Present field to Present.
    • States Text
    • Delay Type
    • Off Delay
    • On Delay
    • Alarm priority
    • Alarm Text
    • Alarm State
    • Alarm Delay
  3. Select the Point Type of the analog input you are using. You can adjust the Value of the Point Type to any of the following:
    • Temperature
    • Humidity
    • CO2
    • Light Sensor
    • Refrigerant
    • Building Pressure
    • Steam Pressure
    • Voltage
    • Current
Note: Voltage and current are fully configurable input types that are meant to be used if a different sensor than what is provided in the VAC1002 accessories list is used. The IOM home page shows the inputs and outputs status and a changeable graphic.