COBP zone setup procedures - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

The Verasys zone controllers come with predefined controllers and are easy to configure when they communicate to the zone coordinator. However, you must configure the following settings to ensure correct operation and control of the connected devices. This section instructs you how to configure the zone controllers for temperature and flow control.

Note: For full wiring details and diagrams refer to the ZEC510 VAV Controllers Installation Guide (Part No. 24-10143-01485).