Testing the unit - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1
Verasys System User Guide
- Product name
- Verasys System
- Document type
- User Guide
- Document number
- LIT-12012371
- Version
- 5.1
- Revision date
- 2024-03-11
- Product status
- Active
- Navigate to the VEC Commissioning page to test the unit.
- Before you turn on the fan, block zones open or ensure the bypass damper is
operational.
- Set the Start Commission parameter to
Trigger.
- Turn on the fan.
- Turn on the heating stages and make sure the SAT increases.
- Turn on the cooling stages and make sure the SAT decreases.
- To finish testing the unit, set the Start Commission parameter back to
Normal.