The Smart Equipment unit comes with partial factory setup completed. Follow this procedure to check that the minimal settings have been performed.
- Log on to the SBH.
- From the device list screen, select the Smart Equipment unit. The RTU home page and the RTU menu structure appear.
- Navigate to .
- Set Rooftop Controller Type to Changeover bypass.
- Navigate to , and verify that Fan Control
Type is set to Single Speed
or Fixed Variable. Fan type can be set to
variable speed without a BYP200 if duct static pressure is conrolled by a variable
speed fan. The RTU requires a discharge air duct static pressure sensor to be
connected and the RTU must have a variable frequency drive.Note: In older versions of Smart Equipment firmware, Rooftop Controller Type is located in the section, and Fan Control Type is located in .
- Check the operation of the unit. Verify that you have some zones blocked open.
- After verifying, see Configuring a COBP damper (BYP200) for flow control to configure the bypass damper.