System settings - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

Use the System Settings menu to adjust the date, time, and timezone. You can also configure the units that appear in the application, and set the BACnet Encoding type for the controllers on the system. When you set the date and time, the SBH sends this date and time to the devices connected to the SBH.

On the System Settings menu, click each of the following icons to adjust the settings:

  1. Click on the calendar icon under the Date heading to select the date.
  2. Click on the clock icon under the Time heading to select the time.
  3. Click the Timezone drop-down list to select the time zone.
  4. Click the Reboot SBH button in system settings menu to reboot the SBH operating system.

The time setting converts the selected 24-hour clock to the standard 12-hour time with AM and PM adjusted. When you adjust the settings and click Save, the time synchronizes to all devices with a time clock. To verify the time synchronized on the devices, navigate to the controller. On the Controller tab, the date and time appears.