SBH updates - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
User Guide
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

Over the air (OTA) updates deploy software updates to the SBH300 from the cloud. OTA updates remove the need for a field technician to update the SBH300 software and the Smart Equipment Control board in a Johnson Controls manufactured rooftop unit. To receive OTA updates, ensure that you connect the SBH300 to the internet. The updates are automatic and require no configuration on the SBH300 local UI. If you are using a building network or building owner provided wireless internet source, make sure that the network allows ports TCP 8096, UDP 10500, and UDP 53 open outbound only.