Software updates - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

Use the Software Updates tab to update the SBH base image firmware operating system (OS) version. This feature can also be used to update the OS version of the SBH. The current software (SW) and dictionary version of the SBH appears on the lower left-hand corner of the screen, under the Verasys logo.

To update the software or dictionary to the latest version, complete the following steps:

  1. Click the Settings tab and navigate to the Software Updates tab.
  2. Click the Choose File button.
  3. Select the .cgi file with the updated software.
  4. Select Upload. The SBH uploads the file and prepares the update. When the upload is complete, the SBH displays Upload Successful.
  5. Select Install.

A red warning bar notifies you that an update is in progress and a countdown begins before the SBH disconnects from the network.

Note: When you update the software, the device retains your previous settings. Set up and update new features before you update the software. When complete, log on to the SBH and take note of the new version number. The SBH SW and OS versions update automatically from JCI cloud services when connected to the Internet, they cannot be updated locally. If the automatic update process does not work, contact Verasys support at http://be-verasyssupport@jci.com. For more information, see SBH updates.