Self-signed certificates and certificates signed by a public certificate authority - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
User Guide
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

A self-signed certificate is a certificate that is signed by the same entity that it certifies. This term does not refer to the identity of the person or organization that actually performed the signing procedure. A self-signed certificate is a certificate signed with its own private key, which means the entity signing the certificate is also the entity that created the certificate.

The SBH ships with a default Johnson Controls® self-signed certificate that provides secure communication. You can only install one certificate on an SBH at a time. When you install a new certificate on a SBH, you overwrite the existing certificate. You can run an SBH on your network with a self-signed certificate.

However, if you need to expose the SBH UI on a public network and have browsers that indicate a trusted site, you must get a signed certificate matching your domain name. You can acquire a valid signed certificate from your IT department or purchase it from a public Certificate Authority (CA) using a certificate signing request (CSR). A certificate signed by a CA is used to establish a secure connection between your browser and the SBH.