Removing a profile from a BACnet device - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
User Guide
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

About this task

Removing a profile from a device removes it from all Verasys features.

To remove a profile from a BACnet device, complete the following steps:

Procedure

  1. Click on the device in the device list and navigate to the Profile view.
  2. Click the Reset to defaults button at the bottom of the page to disassociate the profile from the device and rediscover the device inside of Verasys.