Editing profile configuration - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
User Guide
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

About this task

When you update a profile, you lose all alarm and trend data.

To edit a profile, complete the following steps:

Procedure

  1. Navigate to Settings > Profiles and click the profile you want to edit.
  2. Change the name and the description if needed and click Next to proceed.
  3. When the list of all the objects in the profile appears, follow the same process as in Creating a profile for a BACnet device to modify points. When you are ready, click Save to save the profile.
    Note: When you save the edited profile, it applies to all the devices that used the old profile.