Global shutdown - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

In the global shutdown settings, you can select the device that can initiate a global shutdown of the entire HVAC system. This functionality requires a LC-VAC1000-0 with Verasys Input Output module application installed or LC-VAC1002-0 on the system bus. To set up global shutdown, complete the following steps:

  1. Navigate to the Settings tab.
  2. Click Global Shutdown and choose the device you want to enable for global shutdown.

All devices that participate in global shutdown disable outputs when BI-1 on LC-VAC1002-0 device is closed. Once BI-1 re-opens, the devices return to normal operation.