Device cloning - Verasys - LIT-12012371 - LC-SBH300-0 - Building automation software - Verasys System - 5.1

Verasys System User Guide

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document number
LIT-12012371
Version
5.1
Revision date
2024-03-11
Product status
Active

About this task

Copy configuration parameters to other devices of the same type using device cloning. Refer to the following video link https://docs.jci.com/bas/verasys-clone-controller.

To clone a device, complete the following steps:

Procedure

  1. Navigate to Settings > Clone.
  2. Select a source device from the drop-down list.
    Note: The list contains only the devices that support the cloning feature.
  3. Select a destination device from the drop-down list.
    Note: The choice of devices in the destination devices drop-down list is limited to compatible devices to the source.
  4. Click Clone.
    Note: When you click Clone, a progress bar appears showing how many attributes are successfully cloned.