Before you begin
The SBH300 Wi-Fi Client uses the WPA2-PSK protocol. Ensure that the external Wi-Fi router is set to WPA2-PSK mode.
Do not turn Wi-Fi Client and Ethernet on at the same time. When you use the Wi-Fi Client, make sure that Ethernet is off. To turn off Ethernet, navigate to . From the Enabled list, select Off.